2/13/2012 5:03 AM | |
Joined: 8/31/2010 Last visit: 4/24/2025 Posts: 1525 Rating:
|
Hello Guys, As there are lot ofthreads being discussed on S7-1200 and it's various communication possibilities, I thought of having a thread which is easy to access various pages. To start with a FAQ on With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols support the S7-1200? Application Examples: Communicationwith S7-1200(Wireless Data Communication - GPRS, SMS; TCP) Drive Technology with S7-1200(PROFIBUS DP, USS) Measurement and Sensors with S7-1200(MODBUS TCP / RFID / Code Reading Systems) FAQ on How do you establish MODBUS-RTU communication with STEP 7 Basic V10.5 for the SIMATIC S7-1200?(MODBUS RTU) You guys also can share your experience on this same. |
Last edited by: Ganes10 at: 2/13/2012 5:11 AMLike it? Rate it! |
|
2/13/2012 6:40 AM | |
Joined: 10/7/2005 Last visit: 4/24/2025 Posts: 3047 Rating:
|
I have only one hopefully helpful addition: CPU-CPU communication with SIMATIC controllers (compendium) |
Cheers |
|
Follow us on