11/6/2018 8:49 AM | |
Joined: 4/28/2015 Last visit: 4/19/2025 Posts: 10876 Rating:
|
Hello, generally, S7 communication with PUT/GET can be configured only on one of devices (Client). Other side (Server) has only available DBs or memory which can be accessed from Client. Here is f.ex. example to S7-400: You can define also S7 communication only on S7-1200 and access memory on S7-400. If you check PUT/GET instruction's help, all is described there, what you need set on parameters, how to configure. Example with S7-1200 and S7-300 with S7 communication: S7 communication S7-1200 with S7-300 |
Last edited by: Duris_I at: 11/6/2018 8:51:35 AMLast edited by: Jen_Moderator at: 11/6/2018 10:33:20 AMOptimized links. With best regards... |
|
This contribution was helpful to
2 thankful Users |
11/8/2018 1:25 PM | |
Joined: 8/3/2009 Last visit: 4/17/2025 Posts: 15311 Rating:
|
Hello SPS_AliHariri Here you will find the Basic FAQ to PLC Communication: https://support.industry.siemens.com/cs/ww/en/view/20982954 ByE Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on