10/5/2021 7:40 AM | |
Joined: 7/9/2015 Last visit: 5/29/2024 Posts: 3850 Rating: (564)
|
Hi, it´s possible to run different connection types at the same time with PN Inerface of S7-1200. Please check this: With which devices can the S7-1200 communicate via the integrated PROFINET interface and which protocols does the S7-1200 support?Regards, Towome |
|
|
10/5/2021 8:03 AM | |
Joined: 6/19/2019 Last visit: 5/10/2024 Posts: 694 Rating: (73) |
Why not just put Communication module for modbus TCP? |
10/5/2021 9:12 PM | |
Joined: 3/30/2020 Last visit: 6/7/2024 Posts: 4581 Rating: (951) |
CIP Client – exchanging process data with third party control systems https://support.industry.siemens.com/cs/ww/en/view/109782317 CIP Server – providing process values via CIP with SIMATIC https://support.industry.siemens.com/cs/ww/en/view/109782316 |
Last edited by: qwazee at: 10/06/2021 09:18:12add CIP server Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to2 thankful Users |
10/15/2021 12:31 AM | |
Joined: 12/18/2020 Last visit: 5/23/2024 Posts: 30 Rating: (0) |
Thanks I had seen these posts. I wrote an application using the CIP server. It worked during my bench test, simulating the AB partner with a TP comfort using the AB Ethernet IP driver. I will test the real thing next week and see if it work talking to AB FactoryTalk and with the TP Comfort connected at the same time. I will report. |
Follow us on