7/3/2009 7:20 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello, It would be better to put this issue in wish list thread. Regards, Hristo MIhalev |
This contribution was helpful to1 thankful Users |
7/4/2009 3:46 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
I could not find it.
|
7/12/2009 10:33 AM | |
Posts: 8946 Rating: (999) |
As far as I know, the starter-box is available now, at least in germany. |
7/13/2009 9:54 AM | |
Joined: 5/28/2008 Last visit: 9/11/2024 Posts: 1343 Rating: (141) |
Thanks IBN. It is the picture I have linked in my thread before |
8/4/2009 6:34 AM | |
Posts: 18 Rating: (0) |
I can see some developments in the S7-1200 application area. Have look of the following: http://support.automation.siemens.com/WW/view/en/37604154 |
8/5/2009 8:19 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi all, Yes that starter kit is available. Also a catalog is available as well in printed form as in PDF. |
Smurf |
|
9/4/2009 8:29 AM | |
Joined: 5/28/2008 Last visit: 9/11/2024 Posts: 1343 Rating: (141) |
There is a new application for S7-1200: [url]http://support.automation.siemens.com/WW/view/en/38391227[/url] |
Follow us on