3/24/2018 2:44 PM | |
Joined: 1/2/2017 Last visit: 1/7/2024 Posts: 2 Rating: (1) |
Codesys can communicate with Siemens 1200 via PROFINET, but the firmware version of the 1200 PLC needs to be above 4.0. |
11/13/2018 2:59 PM | |
Joined: 12/16/2012 Last visit: 4/24/2024 Posts: 652 Rating: (130) |
Hi, Is Codesys runing on the RPi? Anyway, first you have to decide which side will be the PN I/O controller and which one the I/O device. If e.g. the RPi will be the I/O device, than you need a s.c. GSDML file, which describes the I/O device and which has to be installed in the PLC's (PN controller) project.
https://support.industry.siemens.com/cs/ww/en/view/91696622/58710581515 If the PLC will be the IO device (better say iDevice), than you need FW 4.0 or higher and install the generated GSDML file in the Codesys project. https://support.industry.siemens.com/cs/ww/en/view/91696622/59264049035 configuration-and-application-of-the-profinet-i-device-function |
Last edited by: Jen_Moderator at: 11/14/2018 9:10:06 AMOptimized links. |
|
This contribution was helpful to2 thankful Users |
4/22/2019 6:04 AM | |
Joined: 1/2/2017 Last visit: 1/7/2024 Posts: 2 Rating: (1) |
我之前发布过一篇文章,我将链接发过来给您。因为这边无法上传文件,实在抱歉 |
12/4/2019 10:08 AM | |
Joined: 4/4/2018 Last visit: 5/29/2021 Posts: 2 Rating: (0) |
Thank you, guy. It works |