12/4/2013 2:08 PM | |
Posts: 51 Rating:
|
Hello everyone, I have S7-1212 DC/DC/Rly with 12MB SD card. I am logging 20 string parameters in one .CSV file. If I set number of records to 255 in DataLogCreate block, the system create's the csv file and datalogger is working. If I set number of records more then 255 (I want't 3000 samples) the system does not create the csv file. Why is this? Best regards |
12/4/2013 3:01 PM | |
Joined: 7/7/2010 Last visit: 3/10/2025 Posts: 15721 Rating:
|
Your strings, are they the default string length (255) or have they been reduced to a realistic size to hold the max content size? @ 255 records with the default string length, that is 1.3 MB per dataset. Are you removing the old dataset before creating a new dataset at the larger size? What error is returned for the create instruction when it fails? |
science guy |
|
12/9/2013 3:56 PM | |
Posts: 51 Rating:
|
Hello, If I don't use STRING then It is no problem. Now I am using INT wich I am writing to my csv. Best regards |
Follow us on