Industry Online Support
Technical Forum
8/23/2014 4:17 AM | |
Joined: 12/16/2006 Last visit: 1/2/2025 Posts: 56 Rating: (2) |
Hi Huggy_d1, Thanks for the quick reply! Does that mean that FW 4 is capable of performing the aforementioned tasks ?
|
8/23/2014 4:26 AM | |
Joined: 7/7/2010 Last visit: 1/14/2025 Posts: 15533 Rating: (2465)
|
No. Sadly all that means is I don't a firmware 4 Plc to test and find out. |
science guy |
|
8/23/2014 4:49 AM | |
Joined: 12/16/2006 Last visit: 1/2/2025 Posts: 56 Rating: (2) |
Hihuggy_d1, Since last post, I have created a TIA project with S7-1200 FW4 and I don't see any difference! I hope it will be supported in the future
|
8/23/2014 8:56 AM | |
Posts: 5225 Rating: (1198) |
I can confirm that the S7-1200 does not handle VARIANT as you would want to. Possibly more than likely on the S7-1500. w |
Follow us on