8/23/2012 10:25 AM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
I have a programm whith OB1 calling twice an FB, each FB with its own DB To debug I can inspect the inputs and outputs of each FB connecting the programm editor on line (screen main.pdf) I can also do the same visualizing the DB of interest. But if I wish to know what happen inside the the FB clicching on the box of OB1 editor the system displays always the FB with the data of the first DB defined and not the data of the DB of the selected FB. Does exists a way to inspect the FB with the data of a selected DB ? AttachmentMAIN.pdf (305 Downloads) |
8/29/2012 11:51 AM | |
Joined: 7/22/2011 Last visit: 12/23/2023 Posts: 78 Rating: (2) |
Hello, all ok but if I wish to see what happen in the FB I cannot select the DB of interest. In the example, I select processo_02 FB but the data are those of processo_01 (DB2 not DB3) AttachmentProcesso_02.pdf (279 Downloads) |
Follow us on