2/22/2016 1:56 PM | |
Posts: 146 Rating: (7) |
Dear Duris, I also tried to configure Write TSAP the same as Read TSAP but without success. I tested it on real PLC in my office. Maybe to configure Write TSAP in some different way!? In attachment there are instructions for S7-1200 for this driver. Thanks for reply! AttachmentSiemens_IO_Driver_manual_S7_1200.pdf (692 Downloads) |
2/24/2016 5:38 PM | |
Joined: 8/31/2013 Last visit: 5/26/2024 Posts: 607 Rating: (41) |
Hello I have a question is it MODBUS communication ? |
Warm Regards |
|
2/24/2016 6:02 PM | |
Posts: 146 Rating: (7) |
Hello! No, it is not a Modbus communication. It is a special driver for s7-1200. On plc side I do not have to configure any protocol, just to enable PUT GET |
Follow us on