7/25/2013 3:17 PM | |
Posts: 74 Rating:
|
According to this press release: And this product description: https://www.automation.siemens.com/mcms/programmable-logic-controller/en/simatic-s7-controller/s7-1200/cpu/pages/default.aspx?HTTPS=REDIRThere should be some great new features, especially the trace function like on the S7-1500 and PLCSIM functionality. But I can't find any order information anywhere. And I can't find any further information than what is contained in the two pages above. Except for the obviously new member 1217C, will the CPU's with the V4.0 firmware then get a new order number? How do you distinguish between a V3.0 and V4.0 when ordering? The Automation Mall doesn't tell anything in the product specifications about firmware version. Will it be possible to upgrade a CPU from V3.0 to V4.0? Or is it new hardware like we had from V2.2 to V3.0? Does anybody know anything about release dates?
|
This contribution was helpful to
1 thankful Users |
8/25/2013 10:20 PM | |
Posts: 32 Rating:
|
This is very good news. I think that the new firmware will come with the new TIA Portal V13. |
10/21/2013 4:52 AM | |
Posts: 3 Rating:
|
I hope the new PORTAL can use STL to programe... |
4/12/2014 8:08 AM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating:
|
follow up question published by t0mekg321is split to a seperate thread with the subjectHow about PLCSIM with S7-1200 and firmware 4.0 ? Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
3/4/2015 2:24 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
|
5/19/2015 11:32 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating:
|
|
Follow us on