4/5/2012 7:20 AM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Hello pethkarashu, Do you have an empty SIMATIC Memory Card? Try this if it canmake your desired outcome. - Recovery from a lost password This is the standard method for Resetting to factory settings. |
Like it? Rate it! |
|
1/25/2013 8:21 AM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Hello RND, Before you download the contents to the PLC, you view the accessible devices and then as shown below double click the "Online & diagnostics" where you can determine the actual Firmware of the CPU. Now set the same firmware of the CPU (also the same MLFB);Make sure the IP address of the PG/PCis in the subnet of the PLCand then try to download, where you should be able to succeed. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
1/25/2013 10:24 PM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Hello RND, Operating System Update for SIMATIC S7-1200 CPU Firmware V3 - http://support.automation.siemens.com/WW/view/en/64789124 Have a look @ this entry, as it says v3.0.2 has a fix for it. |
Like it? Rate it! |
|
9/10/2013 9:08 AM | |
Joined: 8/31/2010 Last visit: 5/21/2024 Posts: 1513 Rating: (223) |
Hello Scotty13, Did you try to perform a factory reset - Resetting to factory settings or thisalternate method. BTW what is the order number of the CPU which you are using. Also mention the firmware version of the CPU. |
Like it? Rate it! |
|
This contribution was helpful to1 thankful Users |
9/10/2013 11:41 AM | |
Posts: 19 Rating: (0) |
thx. I only extract MC from PLC and all is working:) |
This contribution was helpful to1 thankful Users |
5/10/2015 3:18 PM | |
Joined: 4/24/2010 Last visit: 1/24/2024 Posts: 16 Rating: (0) |
Im in same problem How to do "extract MMC from PLC"like you said |
8/26/2015 8:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by plctoan is split to a separate thread with the subject V13 SP1, loading the hardware configuration failed ( 0020-32 20 ). Best regards |
10/6/2015 11:25 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
New question published by thanhbk2001 is split to a separate thread with the subject Error when Compiling Configuration of PLC S7-1200 on TIAportal V13 SP1. Best regards |
Follow us on