2/18/2016 5:42 PM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
I don't have V13 and I don't have 1214C V4 so I can not speak specifically to either one but some common sense tells me that if you were able to connect to a 1214C V4 at home then you're good with Windows 10. A few of things to point out here: 1- Seeing the CPU on "Accessible devices" does *not* mean you are connected. For example I create new project, add unspecified hardware, detect the hardware all of which means that the software can see the device and still not be able to download or upload because of I'm still not connected in a way. The reasons for connection problems are endless. If you go in the project tree and double click on device configuration and then click go online, if you are able to connect you will get a green check mark on the CPU. See attached snap shot. The one on the right is connected and the one on left is not though it is listed in the accessible devices. 2- Separate your uploads, upload the program first and then try to upload the hardware configuration and note down which one gives you the error. 3- Leave changing the IP address till you resolved your connection problems because you have to be connected to be able to change the IP address any way and uploading the program means you are able to connect. I realize your access to the CPUs is limited by geography so it is best to spend lots of time getting to know the software at home with your 1214C and recreate, if you can, connection problems to get to know the software better. Even read in this forum other people's connection problems. Practice taking snap shots of everything you encounter so that when you're onsite you do the same. It helps immensely to see visual clues. William_B posted this link of a "screen capture utility" that I found quite useful. Give it a try. Best of luck |
Follow us on