2/26/2016 5:22 PM | |
Joined: 5/18/2015 Last visit: 11/9/2020 Posts: 67 Rating: (2) |
Hello, Is it still true for S7-1200 firmware v4 PLC's that You can just have one user (admin)? Ive read through the s7-1200 manual (01/2015) and it states "The S7-1200 supports multiple user logins with various access levels (privileges)" (page 789) Trouble is that I can't do it. I mean I've created user, lets say "MIKE" with password "12345" and I did it in the project, then I went online (user list went gray), saved, compiled (Software-all) the project and I downloaded it to the device (Software - rebuild all) Still when I try to acces web page as MIKE I get Invaild Login message. What do I do wrong? I have TIA v13, CPU 1212DC AC DC Rly fw 4.1.3 hw 3 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/29/2016 3:03:21 PMNew subject after splitting |
|
2/29/2016 4:34 PM | |
Joined: 7/7/2010 Last visit: 11/7/2024 Posts: 15388 Rating: (2443)
|
User and web related configuration changes require *hardware* downloads.
|
science guy |
|
Follow us on