11/27/2016 5:45 PM | |
Posts: 3 Rating: (0) |
I can not transfer data from the S7-1200 PLC HMI pro face to the people that can help me? |
11/27/2016 6:29 PM | |
Joined: 9/27/2006 Last visit: 1/2/2025 Posts: 12321 Rating: (2697) |
Hello Prohspecial; Your question is incomplete. What model of Proface HMI do you plan top use? What interface? Ethernet? Look at the information in this Proface technical information webpage, showing which models can connect to S7-1200 (and other families of Siemens PLC) over Ethernet. https://www.hmisource.com/otasuke/download/exdriver/plc/siemens_sies7tcp.htm Notice that there are restrictions on software versions, depending on the moel of Proface HMI selected. Hope thios helps, Daniel Chartier |
11/28/2016 7:19 PM | |
Posts: 3 Rating: (0) |
PLC S7 1200 1214C DC / DC / DC 6ES7 214-1AG40-0XB0 TIAPORTAL V13 PROTOCOL ETHERNET. KHI ĐƯỢC TRUYỀN DỮ LIỆU TỪ HMI Proface THÌ PLC KHÔNG NHẬN TÍN HIỆU Proface |
11/28/2016 7:45 PM | |
Joined: 9/27/2006 Last visit: 1/2/2025 Posts: 12321 Rating: (2697) |
Hello Prohspecial; See if the information provided by Proface in this link can help you out: open the S7-1200 to GP Pro EX sample, https://www.hmisource.com/otasuke/download/sample/gp_3000_m.html Look also at William_B's excellent recommendations in the following discussion on our forum: S7-1200 communication with Proface HMI ???? - Entries - Forum Hope this helps, |
11/29/2016 6:20 PM | |
Posts: 3 Rating: (0) |
CẢM ƠN TẤT CẢ |
Follow us on