5/12/2020 10:01 PM | |
Joined: 12/9/2010 Last visit: 9/18/2024 Posts: 162 Rating: (4) |
Hi, I'm struggling to connect to AWS and I think that some help will be needed. When I try to connect with QDN I get error 809B - The element InterfaceId within the
TCON_xxx structure does not reference a hardware identifier of a CPU or CM/CP
interface or has the value "0". Temporary communication error:
When I try with IP adress and with activateSecureConn FALSE I get error 80C5 The remote partner has terminated the
connection. When I try with IP adress and with validateSubjectAlternateNameOfServer FALSE the "MQTTdata".status.tcpOk turn ON but after a while I get error 80F3 Error during the flag
"keepAlive"
No response from the server
after the KeepAlive was
triggered. I have also tried with both port 8883 and 443
|
Follow us on