6/13/2019 11:23 AM | |
Joined: 3/3/2016 Last visit: 7/15/2024 Posts: 140 Rating:
|
I connect the energy meter (RS-485 port) to CM1241 RS422/485 via Profibus cable. In meter configuration ID -1 BARD RATE- 9.6 PARTY - NONE RS-485 Configuration Port- 269 (as per hardware identifier) BARD - 9600 PARTY - 0 MB_ADDRESS- 1 MODE - 0 DATA_ADDR - 40001 DATA_LEN - 50 DATA_PTR - MD200 Now MB_COMM_LOAD Done= true MB_MASTER Done = false but Busy = true. I have enclosed the image. AttachmentRS-485 IMAGE3.zip (270 Downloads) |
6/13/2019 11:25 AM | |
Joined: 3/3/2016 Last visit: 7/15/2024 Posts: 140 Rating:
|
I cannot read the Data from Energy meter.Kindly update the solution. |
6/14/2019 10:21 AM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating:
|
Hello, try this: |
6/18/2019 3:02 PM | |
Joined: 3/3/2016 Last visit: 7/15/2024 Posts: 140 Rating:
|
MB_Master Busy = true but Value didn't came.I have enclosed the setting snap shot. If any other setting is there. In this meter I had read the value in 30016 address via modbus TCP . METER setting: for remainder Parity - 0 baud - 9600 stop bit -1 ID - 1 AttachmentMB_master.zip (288 Downloads) |
6/18/2019 4:18 PM | |
Posts: 3093 Rating:
|
Hello, Evaluate the outputs of MB_Master in your program: Regards, |
Last edited by: Kaulquappe at: 06/18/2019 16:20:56 |
|
6/18/2019 8:39 PM | |
Joined: 6/14/2013 Last visit: 3/18/2023 Posts: 218 Rating:
|
Hello, with this : |
6/19/2019 11:54 AM | |
Joined: 3/3/2016 Last visit: 7/15/2024 Posts: 140 Rating:
|
Below attach setting ok. |
6/19/2019 12:20 PM | |
Joined: 3/3/2016 Last visit: 7/15/2024 Posts: 140 Rating:
|
Value did't came for above setting |
Follow us on