6/28/2018 12:30 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
|
6/28/2018 12:36 PM | |
Posts: 1283 Rating: (105) |
This photo shows you are reading Input register with address starting in 30001. is it right setting in the PLC?
|
6/28/2018 12:37 PM | |
Posts: 1283 Rating: (105) |
try the address 30001 in the PLC address of MB CLIENT Block. thanks, Jay
|
6/28/2018 12:38 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
AFTER CHANGE CONNECTION type 11 Below result. |
6/28/2018 12:39 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
|
6/28/2018 12:39 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
|
6/28/2018 12:40 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
|
6/28/2018 12:41 PM | |
Posts: 1283 Rating: (105) |
MB DATA Address 30001. This is your address. Not 40001. thanks, jay
|
6/28/2018 12:45 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
can u send any sample project in Third party device via Modbus TCP. |
6/28/2018 12:48 PM | |
Joined: 3/3/2016 Last visit: 10/26/2024 Posts: 140 Rating: (0) |
in Remote address i have given the Converter Mobbus TCP address.Its ok or not. |
Follow us on