7/20/2015 8:03 PM | |
Posts: 75 Rating: (1) |
And this picture about IP adressing.. |
7/21/2015 10:08 AM | |
Posts: 160 Rating: (9) |
Hi, Answering your first question, it only means that if you add 06_processwords in slot 2 of your module, tia expects to find 06_processwords module at slot 2 in the actual module... if you define 06_processwords in slot 4 for example in your actual module it's not going to work... it's only that. Anyway TIA, at least v12.1, defines IOs in automatic once you add all modules in respective slots. and you can find your IO table in this way (photos 1 and 2), note the addresses of input and output bytes. Answering your 2), I'd say that your third-party communication partner (not Siemens but the other) is slave PN partner there for it doesn't matter what ip you want to use because the master (in this case Siemens) is the one who is setting the IP of communication between two modules. Suggestion: leave everything as is do not play with IPs. (be careful not to change your ip of communication between your PC and PLC Siemens, otherwise you will not be able to perform downloading of your project). IPs of Siemens PLC and third-party HW module cannot be the same. (example PLC Siemens IP : 192.168.0.1, for communication between your PC and PLC, Third-party slave module IP: 192.168.0.2. this is valid) Answering your 3), Names are a bit tricky to control therefore once again i'd suggest you to leave everything as is once you introduce your modules in TIA. Once again, until your connection isn't perfect, SF and BF leds will continue to blink. If your profinet connection is OK, BF will stop blinking and you will have only SF always RED. That's because your Siemens PLC isn't in RUN mode. Janko AttachmentPhoto 1 2.DOCX (415 Downloads) |
This contribution was helpful to1 thankful Users |
7/21/2015 10:10 AM | |
Posts: 160 Rating: (9) |
And please, be so kind to share your project for TIA V12 if you are able to. Janko |
This contribution was helpful to1 thankful Users |
7/21/2015 4:07 PM | |
Posts: 5225 Rating: (1188) |
(OFF TOPIC / ENCOURAGEMENT) Caki3000 - Please consider adding star rating(s) the post(s) that helped you most. |
7/21/2015 4:53 PM | |
Posts: 160 Rating: (9) |
I'm glad to be helpful! Enjoy your Profinet !!! Janko |
This contribution was helpful to1 thankful Users |
Follow us on