11/19/2009 5:36 PM | |
Joined: 1/18/2007 Last visit: 8/20/2015 Posts: 16 Rating: (4) |
Also, I dont think you need a dedicated CP. I/O driver with standard ethernet port on the SCADA PC will work fine. |
11/20/2009 10:30 AM | |
Posts: 6 Rating: (0) |
Hi Farlo, many thanks for that Richard |
3/18/2010 4:37 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1424)
|
Hi, The FAQ “How can you establish a connection between a S7-1200 PLC and SIMATIC NET OPC?” http://support.automation.siemens.com/BR/view/en/39960679(Intranet) shows how to communicate with SIMATIC NET OPC. The FAQ Flexible Decoding and Processing of Data Matrix Codes with S7-1200http://support.automation.siemens.com/BR/view/en/40603943 shows how PC Access could also be used. Despite of not 100% homologate, they work with some restrictions. The tip is to program a S7-300/400 connection and gives rack=0 and slot=1. |
Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
5/1/2014 11:29 AM | |
Posts: 12 Rating: (0) |
hi Farlo! can you give me ebook to config it! I'm really have problemwith connect S7-1200 in TIA PORTAL to intouchwonderware |
Follow us on