Industry Online Support
Technical Forum
1/30/2013 1:46 PM | |
Joined: 11/29/2011 Last visit: 2/7/2024 Posts: 11 Rating:
|
Hi I have a jogging question, if I want to use motion control MC_ ... blocks, how to input tag Axis on the block look like, or is there a data type that can be used directly? I have a 1212C CPU, a KT600 HMI and a Bosch Rexroth servo. I need to adjust the speed and ability to change the length. So I want to use the blocks MC_Power, MC_Reset, MC_Halt and MC_MoveVelocity. Or do it with the hardware settings to do? See sending files AttachmentDevice.zip (633 Downloads) |
Last edited by: mrjorgen at: 1/30/2013 3:33 PMExample I All manual formulas förusätter using PTO. But I do not want to use the PTO outputs. Hope that blocks work the same way as the Open PLC blocks? Does anyone know how to do? |
|
1/31/2013 1:54 PM | |
Posts: 267 Rating:
|
Hello, the MotionControl blocks are used for controlling servo or stepmotors via PulseTrainOutput thru a drive. You don't need the drive/motor in your hardware configuration. You have to add a technology object called "axis". And this is your input tag. Perhaps this will help you: http://support.automation.siemens.com/WW/view/en/38391227 |
Follow us on