3/5/2014 5:38 PM | |
Joined: 9/24/2009 Last visit: 4/3/2025 Posts: 16 Rating:
|
How do we get V4 firmware for S7-1200 CPU's ? |
3/5/2014 5:47 PM | |
Posts: 510 Rating:
|
V4 firmware is only available on new 1200 PLCs. Older CPUs cannot be upgraded. Regards, billwest |
3/5/2014 6:03 PM | |
Joined: 9/24/2009 Last visit: 4/3/2025 Posts: 16 Rating:
|
So what do we get with V4 firmware that we don't have in V3 ? |
3/7/2014 3:11 AM | |
Posts: 510 Rating:
|
The details for FW V4 were retrieved from this link: http://support.automation.siemens.com/WW/view/en/69065203 Hereis an excerpt: Withthe new firmware version 4.0 all Simatic S7-1200-CPUs can also be run as Profinet iDevice, in addition to the already available operation as Profinet controller. The new firmware now also offers a trace functionality in real-time for the compact controllers Simatic S7-1200 for application diagnostics and debugging. Until now the trace functionality was only available with the more powerful control systems. A further new feature of firmware version 4.0 is the recipe management that has been implemented on the CPU, which provides the user with recipe data as .csv-file. The access protection against unauthorized project changes has also been enhanced. There are now four security access levels for the CPU access. Updating of already delivered previous generation Simatic S7-1200 controllers (CPU 1211C, CPU 1212C, CPU 1214C and CPU 1215C) to the CPU firmware 4.0 is not possible. |
Last edited by: GrasserF at: 3/18/2014 1:34 PM |
|
3/18/2014 2:32 PM | |
Posts: 510 Rating:
|
Hi, The lastest on firmware V4.0 can be found here: http://support.automation.siemens.com/WW/view/en/86567043 Regards, billwest |
This contribution was helpful to
1 thankful Users |
3/19/2014 3:54 PM | |
Joined: 3/17/2014 Last visit: 8/31/2021 Posts: 31 Rating:
|
Thanks billwest! |
Follow us on