7/22/2015 9:49 AM | |
Posts: 9 Rating: (0) |
Sir, I am using CPU 1214C having MLFCB no. 6ES7 214 - 1AG04-0XB0. Need commissioning support for the following. In the Onboard integrated output Q 0.0 and Q0.1 Is assigned for the Pulse and direction output in the technology objects the function MC-Power, MC-Reset, MC-Jog etc for the third party servo drive. The signal to that device will be via wired. When I executed the Programme using MC-Power ( Servo on enable) and then MC- Jog function to Fwd forced via watch table and the velocity is given. But the problem was there is no response on the drive. kindly advice whether the wiring for the pulse train output and problem execution if any to check the pulse output is alive or not. Application: Pick and place the bearing component using Handling unit. To move left and right movement with different position will work using servo drive ( SMC Electric Servo actuator )and Up and down movement will work using pneumatic cylinder. With best regards, P.Kathirvelu
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 7/22/2015 10:20:14 AMNew subject after splitting |
|
7/22/2015 10:44 AM | |
Posts: 9 Rating: (0) |
Hi, Please see the attached document for your immediate reference. Note : For servo position control use page no. 10 Regards, kathirlat AttachmentLECSA (simplified) (1).pdf (493 Downloads) |
7/22/2015 12:12 PM | |
Posts: 5225 Rating: (1185) |
By default this drive is NPN. |
7/23/2015 1:45 PM | |
Posts: 9 Rating: (0) |
Hi, Please see here with attached PDF for SMC - LECSA servo Actuator using PTO. Kindly advice... AttachmentLEC2-OM026xxim_OperatingManual.pdf (543 Downloads) |
7/23/2015 1:47 PM | |
Posts: 9 Rating: (0) |
Hi, This is next PDF file continous of the previous one attachement AttachmentLEC1-OM026xxim_OperatingManual.pdf (475 Downloads) |
Follow us on