Industry Online Support
Technical Forum
3/7/2013 2:56 PM | |
Joined: 3/28/2011 Last visit: 4/3/2024 Posts: 12 Rating: (0) |
Excellent. Thank you. |
3/7/2013 6:40 PM | |
Posts: 211 Rating: (6) |
For testing purposes, without configured I/Os, there is no need to force variables to test it; just modify it :) |
3/8/2013 9:38 AM | |
Joined: 8/31/2010 Last visit: 4/29/2024 Posts: 1509 Rating: (222) |
Hello huggy_d1, There is a way to have the unused modules in the same project. Have a look at this - Area for unplugged modules |
Like it? Rate it! |
|
This contribution was helpful to2 thankful Users |
Follow us on