6/4/2016 12:07 PM | |
Posts: 8 Rating:
|
Hello, I have a system of the CPU 1513-1 PN and CM PtP RS422 / 485 BA. Send_P2P I use to send data to the slave, but the data is not sent to the CM module output (TX led does not light up and listen to the program (com sniffer) data "does not see". Why Send_P2P does not work? TIA Portal V13 SP1 protocol: freeport (ascii) p.s. translated by google) AttachmentCM_test.zip (1699 Downloads) |
Last edited by: U_eb3317a6-3ccd-4812-b34a-57a5ef080e11 at: 6/4/2016 12:11:24 PMLast edited by: U_eb3317a6-3ccd-4812-b34a-57a5ef080e11 at: 6/4/2016 12:13:20 PM |
|
6/4/2016 5:13 PM | |
Posts: 8 Rating:
|
Maybe somebody has an example of the implementation of the master communication with the slave device on the ascii protocol (freeport). I will be very grateful. |
6/5/2016 9:47 AM | |
Posts: 5225 Rating:
|
@Duris_I, Here is a PDF of the code if it will help you. w AttachmentCM_Test_OB1.pdf (2354 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on