7/27/2017 3:51 PM | |
Joined: 9/27/2006 Last visit: 4/19/2025 Posts: 12346 Rating:
|
Hello SPetkoski; To my knowledge, the S7 family of processors do not support communications with TwinCat processors (neither v2 or v3), and you should look for a gateway between the S7 and the (Beckhoff?) TwinCat PLC. Actually, Beckhoff provides something of interest for a project such as yours: https://www.beckhoff.com/english.asp?twincat/twincat_plc_s5s7_communication.htm The Ethernet adapter the Introduction page points to is from IBH, and it connects the MPI programming port of the S7 CPU to Ethernet (you should not need it with a S7-1500: you can connect directly to TCP/IP; please contact Beckhoff and validate) IBH Link S7++: Ethernet Gateway for the SIMATIC S7-200, S7-300… Hope this helps, |
Last edited by: dchartier at: 7/27/2017 3:56:15 PMLast edited by: dchartier at: 7/27/2017 4:01:46 PMLast edited by: dchartier at: 7/27/2017 4:08:28 PM |
|
Follow us on