10/1/2021 1:24 PM | |
Joined: 9/27/2006 Last visit: 8/15/2024 Posts: 12277 Rating:
|
Hello Satish Kumar; S7 PLCs do not support Ethernet/IP natively, they are designed to work with Profibus and Profinet basically. But recent additions of specialized libraries allow other protocols such as Ehernet/IP to be run on S7-1500 PLCs, using the ntegrated Profinet port of the CPU, for example. This document gives you access to the LCCF_EnetScanner library (and sample code) that allows the S7-1500 to act as an Ethernet/IP scanner: https://support.industry.siemens.com/cs/us/en/view/109782314 Hope this helps, |
Last edited by: dchartier at: 10/01/2021 14:01:08 |
|
This contribution was helpful to
1 thankful Users |
11/1/2021 7:40 AM | |
Joined: 11/29/2019 Last visit: 10/2/2023 Posts: 2 Rating:
|
Hi Dchartier, Searching on this topic I retrieved the sample library from the link you attached. However, it is asking me a password to compile. Do you know if I need to buy this library from siemens? Or is the password provided on another site? Kindly, Ivan
|
1/26/2022 1:37 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, there are application samples for communication over EtherNet/IP: EtherNet/IP Adapter - connecting third-party control systems to SIMATIC S7 controllers via EtherNet/IPEtherNet/IP Scanner – Connecting third party I/O’s using EtherNet/IPAre you having any troubles by using this application samples? Please tell the community were you stuck, otherwise nobody can help you. regards, |
FCK WAR! |
|
10/4/2022 10:47 AM | |
Joined: 12/6/2021 Last visit: 8/12/2024 Posts: 6 Rating:
|
Hello ILMASS and sorry for the late reply, This is the project through which, the S7-1500 controller communicates with Fanuc robot. Best regards!
AttachmentEnetScanner S7_1500-Fanuc.zip (1518 Downloads) |
This contribution was helpful to
10 thankful Users |
Follow us on