10/2/2018 10:51 AM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Your message confuses me a little:
So are you currently using an IOT2000 or a machine running Debian 9? If its not an IOT2000, we will have to split this thread into a different forum.
Having to accept a certificate in UaExpert is normal. If you are able to connect to the OPC UA Server, then everything is fine.
Are you using this package? Cause the current version is 0.2.32 Kind regards! |
10/2/2018 1:00 PM | |
Joined: 9/9/2011 Last visit: 7/5/2024 Posts: 102 Rating: (3) |
Hello i'am sorry if it's not clear. 1) IOT 2000 To resume i'am not using now an IOT 2000 but a real computer using DEBIAN 9. It's in this forum where node-red subjects are more declared. 2) Connection to S7 1500 Like i have mentionned, there is finaly a difference between wago and others OPC UA servers. Each first connection a "trust certificate" is anwser to establish a link. It seem crash on node-red when i try to establish the link. 3) Verison of Node-red. Firstly i have try the last version : 0.2.32 With this version node-red crash at the establishment of the link between the S7 1500 and the computer. I have seen of this forum, it's recommanded to use version : 0.2.16. When i use this version Node-Red don't crash but the message : parseEnpoIntUrl : Invalid enpoint URL opc.tcp::\\192.168.155.23:4840
|
Last edited by: GB002 at: 10/2/2018 1:01:23 PM |
|
Follow us on