5/22/2023 2:11 PM | |
Joined: 5/6/2022 Last visit: 10/4/2024 Posts: 461 Rating: (90) |
Hi mohammed.hussain, I'm afraid that by removing the Memory Card from the 1500 while hot, you have damaged it... Memory Cards cannot be removed without first removing power to the PLC and the 1500s need the Memory Card to function. That's why it doesn't go back to RUN mode. Next, I share two links that will be very useful for you to know how these equipments work: I hope that this documentation that I share with you has been of help to you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
5/22/2023 2:20 PM | |
Joined: 8/16/2022 Last visit: 11/13/2023 Posts: 15 Rating: (0) |
Luckily the card isn't damaged. Thank you for sending the links, I was planning on formatiing the card as well . Which i wont now thanks to the links you have sent, I did manage to get the PLC running again through TIA protal. This is all new to me. Thank you for the help |
This contribution was helpful to1 thankful Users |
Follow us on