1/18/2020 4:17 PM | |
Posts: 1 Rating: (0) |
Hi, I have the same problem with cpu s7-1500. In another project, i used cpu 1200 and in the COMM LOAD block, in the Port assignment option, specify the "PORT" type mark or being system constant. That way the communication was working very well. Now I observed that for the programming of the s7-1500, the constant type PORT is not generated, of which I suppose that it marks the error 16 # 7000 because it does not find the port .. to generate said constant, how could it be done? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2020 11:31:51New subject after splitting |
|