12/6/2019 6:28 PM | |
Joined: 9/9/2014 Last visit: 7/11/2024 Posts: 246 Rating: (40) |
Hello, Read the manual below (so many topics about PLC WEB Server on this forum...): Creating and using user-defined web pages on S7-1200 / S7-1500 Excerpt from the manual (Basics on Creating HTMLs): 1.1.1 Principles of HTML HTML stands for "Hypertext Markup Language" and is a text-based markup language for structuring headers, texts, lists, tables or images. Among other things, HTML does not use loops and variables and is therefore not a programming language. Structure An HTML document consists of three areas: • Document type declaration (DOCTYPE) at the beginning of the file, stating the document type definition (DTD) used, e.g. HTML 4.01 Transitional. • HTML head for information which is not to be displayed in the display area of the web browser.
• HTML body for information which is displayed in the web browser. Excerpt from the manual (Creating User-defined Web Pages on S7-1200 / S7-1500): For access mechanisms via the internet or intranet it is reasonable to use already existing standards, such as, for example, http technology, standard web browsers and common "languages" such as HTML (Hypertext Markup Language) or JavaScript. Excerpt from the manual (Examples for the Web Server): 4.3 Libraries – jQuery and S7 Framework The web pages of the application examples consist of HTML documents, JavaScript files and JavaScript libraries. The file structures can be found in the respective application examples. Some application examples use the “jQuery” and S7 Framework JavaScript
libraries. ********************** According to the manual above - there is no support for PHP (however, you can experiment with it myself) |
Last edited by: Unreality at: 12/06/2019 18:29:00Last edited by: The Helping Hand at: 12/09/2019 16:29:42optimized link Best Regards |
|
12/16/2019 9:24 PM | |
Joined: 2/22/2014 Last visit: 6/21/2024 Posts: 102 Rating: (22) |
No server side languages are available (PHP, Rails, ASP.NET, etc.) |
This contribution was helpful to1 thankful Users |
4/18/2023 6:18 PM | |
Joined: 3/14/2010 Last visit: 7/25/2024 Posts: 19 Rating: (3) |
If anyone hit this threat and want some thing that works check out: phosphor7 Please note to enable PUT/GET and make a DB with optimized block access disabled. |
DIKS automation - https://diks.am |
|
This contribution was helpful to2 thankful Users |
9/1/2023 8:16 AM | |
Joined: 1/12/2023 Last visit: 1/23/2024 Posts: 1 Rating: (0) |
This information helped me a lot, thank you so much. Appreciate it! |
Follow us on