10/15/2019 8:26 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981) |
hello, which version you use? have you read about the important updates for the SW Controller? https://support.industry.siemens.com/cs/ww/en/view/109764666 regards christoph |
10/15/2019 8:32 AM | |
Joined: 3/25/2015 Last visit: 10/30/2023 Posts: 94 Rating: (1) |
CPU 1515SP PC F V2.1 WES 7P 64bit + CPU 1505SP F V2.1 I am reading the content of link your post. And the initial error is the windows 7 black screen after welcome screen, but PLC work well, so I just use DVD which offer within packager to create USB stick, then restore to delievery status with this USB stick. everything is looks fine until I found the PLC con not connected.
|
10/15/2019 11:27 AM | |
Joined: 3/25/2015 Last visit: 10/30/2023 Posts: 94 Rating: (1) |
Dear ChristophD The 2.1 upd7 been installed, but seems the PLC LED RN/ER/MN still dark, the runtime software in win7 indicate messages "CPU volume corrupt, please repair install" I'm try figure out root cause. It progress whatever, thanks a lot.
|
11/8/2019 11:55 AM | |
Joined: 4/28/2015 Last visit: 11/5/2023 Posts: 13 Rating: (0) |
|
6/11/2021 11:38 AM | |
Posts: 5 Rating: (0) |
Can you please share the solution? I'm fighting the same problem |
Follow us on