1/3/2016 8:11 AM | |
Posts: 53 Rating: (1) |
Dear Boss, I had a PLC with this part no. 6es7214-1bd23-0xb0. There was also two analog module. Last time PLC was faulty. Power supply burn. So, I bought a new PLC with same part no and downloaded the old program to new PLC. When I run the machine the digital bit work if I command from HMI. LIke off on. But If a set a analog value from value HMI its not working. (The HMI giving data to PLC with this variable: VW106. If I give a value manually like 32000 this give 10v to analog output. ) I have attached the program here. AttachmentProject1.zip (572 Downloads) |
5/18/2016 10:12 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by Automation_1987 is split to a separate thread with the subject Siemens interview questions. Best regards |
Follow us on