1/9/2007 12:01 PM | |
Posts: 3 Rating: (0) |
hello everybody....i have a question....how can i configure a s7-200 from begining ...sorry i am new to this and i need some help. thanks, adriana pop |
1/9/2007 3:56 PM | |
Joined: 9/23/2005 Last visit: 8/13/2024 Posts: 4347 Rating: (1439) |
Hi, you can find some help in the s7-200 manual: http://support.automation.siemens.com/WW/view/en/1109582 See chapter 2. |
Denilson Pegaia |
|
1/12/2007 9:40 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi popadrianadorina, From the beginning... You can find information about the s7-200 in the catalog ST70. That catalog and other can be ordered or downloaded from The Information- and Download Center. At this moment you shouls download/order the ST70-2007 catalog and maybe the HMI catalog (ST80-2006 and ST80 news-2007) You should also download theS7-200 manual. [quote user="Pegaia"]Hi, About powersupplies, you can use any powersupply (also non-Siemens, e.g. Riedel) as long as it is suitable for the S7-200/300, e.g.for 24VDC you should use a switched-mode powersupply because of the small tolerance. For a 'short' description of the modules you can use the catalog and chapter 1 of the manual. More detailed information can be found in appendix A of the manual. When configuring/planning a station pleas note table 1-2 of the manual where the amount of expansion modules is mentioned. Is this what you mean? Good luck. |
Smurf |
|
Follow us on