7/27/2011 12:42 PM | |
Joined: 3/21/2006 Last visit: 7/26/2024 Posts: 10228 Rating:
|
Hello, In order to use a profibus slave is needimng a GSD file. In Simatic Manager you should assign a Profibus address which must be the same as gataway configuration. All the settings is according to http://www.asconcorp.com/library/pdf/delta2/DX_Programming.pdf There you should assign where will be send the temperature (which word/byte) in order Profibus Master (S7-300) to know where to read it. Best regards, Hristo Mihalev |
This contribution was helpful to
1 thankful Users |
Follow us on