5/25/2007 12:15 PM | |
Posts: 3 Rating:
|
I'd like to find out from which S7-300 CPU one can run CFCs. I also have FBs with the alarm_8p block. From which CPU is this supported? |
5/26/2007 10:10 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi, Only ALARM_S and look alikes can be used in a S7-300, see also the SFC/SFB that can be used in a S7-300. 1. S7 300
This is only a guideline. Message might well be lost earlier on if the messages are sent to quickly one after the other. The return value RET_VAL then returns 8082.
|
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on