3/18/2024 7:42 AM | |
Joined: 2/19/2024 Last visit: 3/19/2024 Posts: 3 Rating: (0) |
Hi all , im new to plc programing. We have a couple of S7-300 cpus at work. been able to program the cpu 6ES7 314-6CG03-0AB0 without any issues . but now trying to connect to at ET200s 151 1BA02 0AB0, which i have tried many things and cant get simatic manager or tia portal to see it. im using a profibus cable which is connected to the incoming of each connecter and the switch is in the off position. will post the buffer diagnostics but they don't mean much to me thanks AttachmentDiagnose.txt (26 Downloads) |
Last edited by: Liam12299 at: 03/18/2024 08:17:32 |
|
3/18/2024 8:01 AM | |
Joined: 2/19/2024 Last visit: 3/19/2024 Posts: 3 Rating: (0) |
thanks for reply. what do you mean set entries to in example 499? and oops i meant they are both set to on thanks |
3/18/2024 8:18 AM | |
Joined: 2/19/2024 Last visit: 3/19/2024 Posts: 3 Rating: (0) |
changed the setting in diagnostic buffer, files should show more now thanks |
Follow us on