9/9/2013 9:31 AM | |
Posts: 1064 Rating:
|
It shows maximum 1 2with 8 free i do have2 op panels on profibus but that is it .I t say i have 8 reserved for s7 communications and 0 used |
9/9/2013 11:24 AM | |
Joined: 4/24/2006 Last visit: 4/18/2025 Posts: 8956 Rating:
|
Hello playerslight, Ok, you are using an older CPU. Then you have 4 static connections, and 8 dynamic connections. But when you are using the 4 static connections, you can not reach CPU. Try to disconnect an OP panel (for test) and perhaps then you can connect WinCC. If this helps, then perhaps you can update the firmware: Operating system updates for S7-315 CPUs Or change CPU for newer one. Best regards, Wizard |
This contribution was helpful to
2 thankful Users |
Follow us on