6/17/2024 9:17 AM | |
Joined: 3/15/2017 Last visit: 6/17/2024 Posts: 5 Rating: (0) |
Hi there, I am using 6ES7317-2AK14-0AB0 on my stenter Machine. Suddenly the machine stopped. And the cpu don't have any lights. I checked the supply 24vdc was ok. Then after 12/13 hours machine was without power. After that when we power on again the cpu had light and it was good condition but its configuration got default. Same things happens after 5 days again. Can anyone help me with this issue please ?? ? If the fuse fried how it can on after some hours?? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/17/2024 13:22:16New subject after splitting |
|
6/20/2024 9:09 AM | |
Joined: 7/19/2022 Last visit: 6/28/2024 Posts: 373 Rating: (61) |
Hello For My Job, If during operation all the lights on the S7-300 go out or the power supply is not working properly or the PLC has an internal fault, I would first try to change the power supply and if not, it will be necessary to repair the S7-300. |
If this Information really helps, you could use the Rate function |
|
Follow us on