4/4/2016 7:51 AM | |
Joined: 12/23/2015 Last visit: 1/16/2023 Posts: 43 Rating:
|
Hello, Thanks for your replay. Pls see the attach diagnostics buffer.This diagnostics buffer is not taken on same time which i am described before. I can not attach here the diagnostics buffer at the same time of our problem date because that time i was not present at our plant. I also notice MMC of cpu used 88% of memory. Is it caused the problem? AttachmentDiagnose.txt (997 Downloads) |
4/8/2016 9:53 PM | |
Joined: 8/31/2013 Last visit: 5/26/2024 Posts: 607 Rating:
|
Hello I see you have Master-Slave communication ,,,as I understand you case you did not use OB 86 you can see the attached file I hope it will help you AttachmentCpu317-2-Ether-Profi.zip (886 Downloads) |
Warm Regards |
|
4/12/2016 9:43 AM | |
Posts: 144 Rating:
|
Hi While trying to figure out the problem of slave no.8 you can download mentioned OB(86) into cpu to prevent stop mode! |
Follow us on