7/20/2024 2:36 PM | |
Joined: 4/28/2015 Last visit: 7/25/2024 Posts: 14 Rating:
|
Hi Daniel, Glad to receive your assistance here Now the system is healthy it might be caused by an external signal. But I am still having issues to upload the full program to PG. First I could not verify the right TIA portal, I tried to check it under Online & Diagnostics / General tab but I could not see TIA portal version there. When I tried version 12 and then tried to upload both software and hardware I ended up with the following error '' The online module 6ES7 315 2FJ14 0AB) V3.2 does not support uploading to PG which as far I I knew it is related to issues in the software version I am using. AttachmentTIA error.zip (80 Downloads) |
7/20/2024 3:07 PM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating:
|
Hello, May be it is programmed with Simatic Manager! |
Ayman Elotaify |
|
7/21/2024 9:11 AM | |
Joined: 5/28/2008 Last visit: 9/9/2024 Posts: 4515 Rating:
|
Hello, I think the followings will help you: TIA Portal: Which Version? How to find which version was used on your PLC: 3 different ways |
Ayman Elotaify |
|
7/21/2024 11:03 AM | |
Joined: 4/28/2015 Last visit: 7/25/2024 Posts: 14 Rating:
|
Aymen ,, I could not find (Version of the TIA portal project) and instead I found (Firmware Expansion). |
Follow us on