11/13/2007 6:27 AM | |
Posts: 22 Rating: (0) |
Dear All, I have a system in which I am using S7-300 CPU 315-2DP Telecontrol Moddule VICOS RTU TIM 3V BN (MLFB No. 6NH7808-3AA00) with some remote I/O & profibus network . Now I want to upgrade the system to S7-300 software redudedant. (S7-300 R) using siemens software FB's. I considered two CPU 315 - 2DP IM153-2 redudant bundle. But the TIM module is not confirable in IM station. Is I need to procure Two different TIM modules? Then How they will be configured at SCADA ? Please let me what will be my new System Configuration?. I am attaching my present system Configuration. Thanx & Regards, Praveen Patil AttachmentBMF System.pdf (518 Downloads) |
Follow us on