7/5/2017 9:04 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, wireless? with a distance of around 1 km? I don´t think that this is possible. regards, |
FCK WAR! |
|
1/1/2020 7:36 AM | |
Joined: 7/30/2018 Last visit: 3/31/2022 Posts: 1 Rating:
|
Hi Niranjankmr888, I am sure you have found a solution by now, but I can share what we have done for wireless connection between Siemens PLC's. We used 5GHz radios (with Ethernet interface) and PLC to PLC communication setup. The distance between PLC's is close to 2km and the connection is very stable for the last 3+ years now. Link to the radio website: https://www.tp-link.com/en/business-networking/outdoor-radio/cpe510/?utm_medium=select-local Hope this helps. Kind regards, Stephan |
This contribution was helpful to
1 thankful Users |