9/2/2009 9:48 AM | |
Posts: 2 Rating: (0) |
Only for test purpose, is possible to use a S7-300 CPU without micro memory card? i.e. load hardware configuration and test I/O. Thanks in advance. |
9/2/2009 9:56 AM | |
Joined: 5/28/2008 Last visit: 10/12/2024 Posts: 4515 Rating: (839) |
Dear manmorcar, If you are using the new type of S7-300 CPUs, Then the answer is NO. If you opened the CA01 Mall, you will found the following statement in the over view of each CPU: Micro memory card required for operation of CPU. And also the CPU won't go to run mode if the MMC is not inserted into its bay. |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
9/2/2009 10:20 AM | |
Posts: 2 Rating: (0) |
|
This contribution was helpful to1 thankful Users |
Follow us on