8/2/2022 8:29 PM | |
Joined: 8/2/2022 Last visit: 12/16/2022 Posts: 1 Rating:
|
We use Siemens S7 300 . One of the blocks does not turn on. Stays in stop mode all the time. Please help . |
8/3/2022 7:21 AM | |
Joined: 1/21/2013 Last visit: 8/1/2024 Posts: 3043 Rating:
|
Hi Omen22, even if it is not clearly visible in your image, I assume the switch is in position RUN. In this case, the LEDs the image is showing will not help to solve your issue. At least you will have to read out the diagnostics buffer. For this, you will need the engineering software (STEP 7 V5.x or STEP 7 TIA Portal ≥ V12) or the SIMATIC Automation Tool. For the engineering software you will need a license (without a license you can use a 21-day trial), the SIMATIC Automation Tool is for free. In both cases, you will need a registration for the authorization to download export restricted software. Before downloading a software, please take a look at the ordering number of the PLC. STEP 7 TIA Portal and the SIMATIC Automation Tool can only be used with the current and the direct previous generation. In case of SIMATIC Automation Tool the supported PLCs are 6ES7 314-6EH04-0AB0, …315-2EH13-0AB0, …315-2EH14-0AB0, …315-2EH14-0AB0, …315-2FH13-0AB0, …315-2FJ14-0AB0, …315-2FJ14-0AB0, …317-2EK13-0AB0, …317-2EK14-0AB0, …317-2EK14-0AB0, …317-2FK13-0AB0, …317-2FK14-0AB0, …317-2FK14-0AB0, …318-3EL00-0AB0, …318-3EL00-0AB0, …318-3EL00-0AB0, …318-3EL01-0AB0, …318-3FL00-0AB0, …318-3FL00-0AB0, …318-3FL00-0AB0, …318-3FL01-0AB0. Kind regards |
Follow us on