6/28/2010 2:51 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating:
|
I have a program in the CPU, which is total of less than 1MB size, when I download the program in CPU memory, it works fine. However I also want to save theArchived program in PLC memory, when I save the program in memory card, it does not accept and mentions the space in the memory card is zero. I calculated and found that the zip file size is only 790KB, and PLC memory has only 1MB of program. IS there any way I can also save theArchivedprogram, or memory card is not functioning properly. |
6/28/2010 3:10 AM | |
Joined: 9/27/2006 Last visit: 4/4/2025 Posts: 12345 Rating:
|
Hello lucky; What is the size of the MMC you are using now? What function do you use to transfer the data (zip file) to the MMC? Hope this helps, Daniel Chartier |
6/28/2010 4:43 AM | |
Joined: 10/7/2005 Last visit: 4/6/2025 Posts: 3046 Rating:
|
Hello Lucky123 the following two FAQ's, may (hopefully will) help too: S7-300: How can I find out the size of the MCC so I can store my whole STEP 7 project on it? How can you load projects to a memory card and back again to a PG/PC? |
Cheers |
|
This contribution was helpful to
1 thankful Users |
6/28/2010 5:00 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating:
|
Hello Fritz and Dchartier, I checked the zip(archived) file size in explorer is about 600KB and the total size of the memory card which I am using is 2 MB, and if I see the load memory area then it is about 1MB. I see no reason why the Archived file should not be able to be saved in memory card, however since I have not much experienced such types of issue, hence I thought of sharing this information on the forum and find out what can be the reason. I am yet to find the cause and solution for this problem. Let me know if I can provide some more information. Thanks, |
6/29/2010 3:40 AM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating:
|
Hello Experts,
I am still waiting the response to get this resolved. Please provide your valuable inputs. Thanks, |
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on