Industry Online Support
Technical Forum
3/3/2008 7:23 PM | |
Posts: 54 Rating: (3) |
The question is WHAT interface may I use?..Could it be PN or MPI only (through USB-MPI adapter)? |
3/4/2008 7:35 AM | |
Posts: 2348 Rating: (263) |
You can find online updating procedure here http://support.automation.siemens.com/WW/view/en/23992548 As i understood you can useanyinterface. |
12/22/2011 11:30 AM | |
Posts: 27 Rating: (1) |
Hi Kevlar! I don't know exactlywhy there are 3 data files into the firmware update. I think the KOMP_1.UPD is the update file and CPU_HD.UPD is needed to make a update-MMC.For the online update is this not important, because you "have selected a file". description: http://support.automation.siemens.com/WW/view/en/44442927 |
Follow us on