4/26/2016 6:40 PM | |
Joined: 3/17/2013 Last visit: 12/19/2024 Posts: 481 Rating: (43) |
Hi, Forcing DO should not cause any EXTF OR SF. Could you upload diagnostic buffer Vijay |
4/27/2016 12:52 AM | |||||||||||||||||||||||||
Joined: 7/2/2008 Last visit: 9/30/2024 Posts: 928 Rating: (309) |
Hello, As explained by Ibrahim, The FORCE function is part of "testing and commissioning functions". These functions inhibit link-up and update. So, you should disable FORCE functions before you proceed to put CPUs in redundant mode. Table: Properties of link-up and update functions
Best regards, H-H |
||||||||||||||||||||||||
This contribution was helpful to4 thankful Users |
4/27/2016 4:15 PM | |||||||||||||||||||||||||
Joined: 9/22/2014 Last visit: 6/12/2024 Posts: 89 Rating: (13) |
Hello, Thanks H-H ,That was helpful. Thanks, Pratts23. |
||||||||||||||||||||||||
Follow us on