Industry Online Support
Technical Forum
2/10/2010 2:46 PM | |
Posts: 96 Rating: (7) |
Dear Wincc,
Let me summarize your problem by these words: "When the Master/Reserve CPUs are switched the connection in Wincc is lost." What your procedure at Wincc side ? I think you did not do any thing there, because you did not say anything about that. So, see the attached file it will help AttachmentSWR_WINCC_english.pdf (159 Downloads) |
2/11/2010 5:57 AM | |
Joined: 6/3/2009 Last visit: 10/24/2024 Posts: 101 Rating: (7) |
Dear Raednabeel S7 system to Wincc connection has no Problem.Master Reserve SwitchOver time Wincc is communicating. Fine When CPU has some problem Reserve PLC takecare andWincc is communicating to CP(Reserve PLC) and Vise-versa. When Master IMhas some problem Reserve PLC and it's IM takecare andWincc is communicating to CP(Master PLC) and Vise-versa. Why ? But Wincc Communication is not lost all parameters are visiable and working fine. |
Follow us on