5/3/2008 1:50 PM | |
Posts: 11 Rating: (0) |
we have configured the hardware for S7-400 F/H system.in address overview we are finding the module repetation with different address.Please find attached file and the repetation is marked with arrows. also we are not able to remove the same module from configuration as after that comilation is not possible. AttachmentPresentation1.zip (375 Downloads) |
5/5/2008 12:11 PM | |
Posts: 11 Rating: (0) |
We have observed the file after Reorganize and Save as but the problem remains same. Attachmentsimatic h station(1).zip (298 Downloads) |
5/5/2008 5:10 PM | |
Posts: 2661 Rating: (279) |
MRK: When you did a save-as with reorganization, did you change the name of the project? It is very important that you change the name since for certain type of problems in the project it is not enough to save-as with the same name in a different folder. See step 1 in the following FAQ: Why does the message "S7tgtopx.exe has caused an error and will be closed" appear? http://support.automation.siemens.com/WW/view/en/13770987 Let me look at your other problems. Regards, Phantom |
5/5/2008 8:35 PM | |
Posts: 2661 Rating: (279) |
MRK: AttachmentDokument1.pdf (338 Downloads) |
Follow us on