7/10/2013 12:38 PM | |
Posts: 515 Rating: (56) |
hi, which i/O modules are you using? is it s7 300 modules or s7 400 modules? you can use expansion racks to connect multiple modules.
|
7/10/2013 5:47 PM | |
Joined: 10/19/2012 Last visit: 4/17/2022 Posts: 315 Rating: (9) |
The best way will be to use ET200M & distributed IOs. . if you don't seem it feasible then above posts might help. . |
7/11/2013 12:33 PM | |
Posts: 515 Rating: (56) |
hi, find the attached architecture which might help you.
AttachmentS7 412-5H ARCHITECTURE.pdf (431 Downloads) |
7/11/2013 1:01 PM | |
Joined: 5/28/2008 Last visit: 5/26/2024 Posts: 4506 Rating: (836) |
Hello, If you are willing to use S7-400 IOs, please note the following points:
Two Options are possible:
Please note that standard PS is different than PS suitable for redundant operations. Here's bellow an example:
Hope this helps. Attachmentbrochure_simatic-controller_en.pdf (279 Downloads) |
Last edited by: Ayman Elotaify at: 7/11/2013 1:02 PMAyman Elotaify |
|
This contribution was helpful to1 thankful Users |
7/11/2013 1:07 PM | |
Joined: 5/28/2008 Last visit: 5/26/2024 Posts: 4506 Rating: (836) |
Dear both Shazin and Ahmed, To finalize this subject.
Hope it will helps. |
Last edited by: Ayman Elotaify at: 7/11/2013 1:11 PMAyman Elotaify |
|
This contribution was helpful to2 thankful Users |
Follow us on